AXIS#.MT.DISALLOWZEROSTARTVEL

Description

This parameter sets the motion task control word specifying whether or not the starting velocity of the task can be 0.

It takes the following values:

Value Description
0

Non-zero start velocity disallowed

1 Non-zero start velocity allowed

Examples

Usage

This keyword is used to set what you would otherwise have set with AXIS#.MT.CNTL.

Code

MT.NONZEROSTARTVEL 0 1 Will configure Motion Task 0 to allow non-zero start velocity.

Context

See AXIS#.MT.CNTL for more information on the argument semantics.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type Read/Write Array
Units N/A
Range 0 to 1
Default Value 0
Data Type Integer
See Also AXIS#.MT.CNTL

Stored in Non-Volatile Memory

No

Variants Supported

Supported on all drives.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.MT.DISALLOWZEROSTARTVEL 0

50dfh

01h

Unsigned8

-

-

Read/Write

No

AXIS1.MT.DISALLOWZEROSTARTVEL 1

50dfh

02h

Unsigned8

-

-

Read/Write

No

AXIS1.MT.DISALLOWZEROSTARTVEL 2

50dfh

03h

Unsigned8

-

-

Read/Write

No

AXIS1.MT.DISALLOWZEROSTARTVEL 3

50dfh

04h

Unsigned8

-

-

Read/Write

No

AXIS1.MT.DISALLOWZEROSTARTVEL 4

50dfh

05h

Unsigned8

-

-

Read/Write

No

AXIS1.MT.DISALLOWZEROSTARTVEL 5

50dfh

06h

Unsigned8

-

-

Read/Write

No

AXIS1.MT.DISALLOWZEROSTARTVEL 6

50dfh

07h

Unsigned8

-

-

Read/Write

No

AXIS1.MT.DISALLOWZEROSTARTVEL 7

50dfh

08h

Unsigned8

-

-

Read/Write

No

AXIS1.MT.DISALLOWZEROSTARTVEL 8

50dfh

09h

Unsigned8

-

-

Read/Write

No

AXIS1.MT.DISALLOWZEROSTARTVEL 9

50dfh

0ah

Unsigned8

-

-

Read/Write

No

AXIS1.MT.DISALLOWZEROSTARTVEL 10

50dfh

0bh

Unsigned8

-

-

Read/Write

No

AXIS1.MT.DISALLOWZEROSTARTVEL 11

50dfh

0ch

Unsigned8

-

-

Read/Write

No

AXIS1.MT.DISALLOWZEROSTARTVEL 12

50dfh

0dh

Unsigned8

-

-

Read/Write

No

AXIS1.MT.DISALLOWZEROSTARTVEL 13

50dfh

0eh

Unsigned8

-

-

Read/Write

No

AXIS1.MT.DISALLOWZEROSTARTVEL 14

50dfh

0fh

Unsigned8

-

-

Read/Write

No

AXIS1.MT.DISALLOWZEROSTARTVEL 15

50dfh

10h

Unsigned8

-

-

Read/Write

No

AXIS1.MT.DISALLOWZEROSTARTVEL 16

50dfh

11h

Unsigned8

-

-

Read/Write

No

AXIS1.MT.DISALLOWZEROSTARTVEL 17

50dfh

12h

Unsigned8

-

-

Read/Write

No

AXIS1.MT.DISALLOWZEROSTARTVEL 18

50dfh

13h

Unsigned8

-

-

Read/Write

No

AXIS1.MT.DISALLOWZEROSTARTVEL 19

50dfh

14h

Unsigned8

-

-

Read/Write

No

AXIS1.MT.DISALLOWZEROSTARTVEL 20

50dfh

15h

Unsigned8

-

-

Read/Write

No

AXIS1.MT.DISALLOWZEROSTARTVEL 21

50dfh

16h

Unsigned8

-

-

Read/Write

No

AXIS1.MT.DISALLOWZEROSTARTVEL 22

50dfh

17h

Unsigned8

-

-

Read/Write

No

AXIS1.MT.DISALLOWZEROSTARTVEL 23

50dfh

18h

Unsigned8

-

-

Read/Write

No

AXIS1.MT.DISALLOWZEROSTARTVEL 24

50dfh

19h

Unsigned8

-

-

Read/Write

No

AXIS1.MT.DISALLOWZEROSTARTVEL 25

50dfh

1ah

Unsigned8

-

-

Read/Write

No

AXIS1.MT.DISALLOWZEROSTARTVEL 26

50dfh

1bh

Unsigned8

-

-

Read/Write

No

AXIS1.MT.DISALLOWZEROSTARTVEL 27

50dfh

1ch

Unsigned8

-

-

Read/Write

No

AXIS1.MT.DISALLOWZEROSTARTVEL 28

50dfh

1dh

Unsigned8

-

-

Read/Write

No

AXIS1.MT.DISALLOWZEROSTARTVEL 29

50dfh

1eh

Unsigned8

-

-

Read/Write

No

AXIS1.MT.DISALLOWZEROSTARTVEL 30

50dfh

1fh

Unsigned8

-

-

Read/Write

No

AXIS1.MT.DISALLOWZEROSTARTVEL 31

50dfh

20h

Unsigned8

-

-

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

6315

1

6315 (0x18ab)

AXIS1.MT.DISALLOWZEROSTARTVEL

Unsigned8[32]

Read/Write

Yes

71851

2

6315 (0x18ab)

AXIS2.MT.DISALLOWZEROSTARTVEL

Unsigned8[32]

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS1.MT.DISALLOWZEROSTARTVEL

6315

Unsigned8[32]

Read/Write

-